Uncorrected Flow Volume Today

Associated with: Flow runs

This attribute indicates the uncorrected gas flow volume so far, during the present contract day. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller, if that Flow Run performs AGA-7 Flow Calculations. The units that apply to the attribute depend on the Measurement Units system being used for the Flow Run’s Contract Units.

Example:

12.45
(for uncorrected gas flow volume in E3m3 (or 103m3))


Disclaimer

ClearSCADA 2017 R3