Water Cut Properties (Liquid Flow Run)

The fields within this section of the Liquid tab display those properties that are associated with Water Cut measurement. The 'water cut' is the term used to describe how much of the total liquid is oil or water. This is usually specified as a percentage that indicates how much water is in the liquid.

You can configure these properties directly in ClearSCADA, or read the configuration into the ClearSCADA database (see Configure or Read the Flow Run Configuration).

 

The input alarms fields within the Water Cut section enable you to set the alarm thresholds for alarm types that have been enabled in the Inputs section of the Flow Run tab.

Use the following to configure alarm limits in the Water Cut section:

 

The following properties only apply when the Water Cut Mode (see above) is set to 'Inferred Water Cut':

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

ClearSCADA 2017 R3