SCADAPack x70

Configure the HART Pass Through

The HART Pass Through section of the Settings tab allows you to define whether the SCADAPack x70 device and the 6602 HART module send data from HART instruments directly to an Asset Management System (AMS or HART Communication DTM).

Use the following to configure the HART Pass Through feature:

Enabled

For the SCADAPack device to discover HART devices connected to a 6602 module, for device scanning, or for a HART Pass Through operation, you need to enable the 6602 to discover active HART devices.

You need to add a HART_6602Control function block in the SCADAPack x70 Logic Editor to enable device discovery and provide control over the scanning process. A separate HART_6602Control function block is required for each 6602 HART module connected to the SCADAPack x70 device.

Listen Port

You need to enter the TCP port on which the SCADAPack x70 device listens for connection requests from the AMS or HART Communication DTM when HART Pass Through is enabled. Default port is 5001.


Disclaimer

ClearSCADA 2017 R3