SCADAPack x70

Define the Minimum Number of (Buffered) Events

The fields within the Unsolicited Message Generation (Buffered Events) section of the tab apply to unsolicited messages that the outstation sends to any DNP3 master. If an outstation is to send unsolicited messages, in addition to the fields in this section, you also have to configure the properties within the Connection to Master section of the tab.

Use the fields within the Unsolicited Message Generation (Buffered Events) section of the DNP3 Slave tab to specify for each class type the minimum number of events that are stored in the outstation's internal buffer before they are sent as unsolicited messages.

Class 1 Minimum Events

Specify the minimum number of Class 1 events that have to be stored in the SCADAPack x70 device’s internal Event Buffer, before the outstation attempts to send an unsolicited message. Default is 250.

Class 2 Minimum Events

Specify the minimum number of Class 2 events that have to be stored in the SCADAPack x70 device’s internal Event Buffer, before the outstation attempts to send an unsolicited message. Default is 250.

Class 3 Minimum Events

Specify the minimum number of Class 3 events that have to be stored in the SCADAPack x70 device’s internal Event Buffer, before the outstation attempts to send an unsolicited message. Default is 250.


Disclaimer

ClearSCADA 2017 R3