SCADAPack x70

Device Configuration IP Communications Tab

The IP Comms tab allows you to configure IP communication between the SCADAPack x70 device and another device.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

WARNING

communication loss

Applying invalid communication parameters can lead to loss of communication between ClearSCADA and your SCADAPack x70 device or between devices.

Before changing communication parameters, verify that the new settings are valid for this device and valid in your network.

Failure to follow these instructions can result in death or serious injury.

Disclaimer

ClearSCADA 2017 R3