Display Outstations
Associated with: SCADAPack x70 Firmware Image items
Security permission required to access this pick action: Read
Use this pick action to display a Queries List of the SCADAPack x70 Device Configuration items with which the selected Firmware Image database item is associated. The List indicates the devices on which the operating system firmware can be updated using the .biz file that was last uploaded into ClearSCADA using this particular Firmware Image item.
The Display Outstations pick action is not a method and therefore cannot be used with the automation interface.