Downloaded Firmware Image
Associated with: SCADAPack x70 DNP3 Outstations
This status attribute indicates:
- The name of the last .biz file to be downloaded to the SCADAPack x70 device.
- A time stamp showing the last modification date and time of the .biz file from which the downloaded Firmware Image file was obtained.
The attribute is only displayed if the Download Firmware pick action has been used to successfully download an operating system firmware file to the SCADAPack x70 device. (Each firmware file comprises a .biz file that has been imported into ClearSCADA using a SCADAPack x70 Firmware Image database item.)
"911e57x.biz" Modified at 2018-05-29 10:05:32
(Indicating that the last Firmware Image file to be downloaded to the SCADAPack x70 device was the file named ‘911e57x.biz’. The .biz file from which the Firmware Image file was obtained was last modified on the date and time indicated above.)
Further Information