SCADAPack x70

Firmware Download Alarm

Associated with: SCADAPack x70 DNP3 Outstations

This status attribute indicates whether ClearSCADA's last attempt to Download Firmware was unsuccessful.

An existing firmware upgrade alarm is cleared when ClearSCADA next updates the operating system firmware successfully.

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R3