Import from RemoteConnect
Associated with: SCADAPack x70 Device Configuration items
Security permission required to access this pick action: Control
Use the Import from RemoteConnect pick action to import configuration and/or SCADAPack x70 logic from SCADAPack RemoteConnect configuration software into ClearSCADA for the selected SCADAPack x70 device. You might choose to do this, for example, if you want to use ClearSCADA to configure a SCADAPack x70 device and want to use SCADAPack x70 logic in that device.
To import configuration and/or logic for the selected SCADAPack x70 device from RemoteConnect:
- Select the Import from Remote Connect pick action.
The Import from RemoteConnect dialog box is displayed.
- Select the browse button next to the File Name field.
A File Name window is displayed. Its layout varies, depending on the operating system that you are running. - Use the window to locate and select the file that you want to import from RemoteConnect. This will typically take the form of a SCADAPack x70 manifest configuration file (.rtz file).
- Select the OK button to confirm the details and import the selected file.
The manifest configuration file is imported and made available to ClearSCADA. Checks are run to compare the content of the imported manifest with the configuration that exists in the ClearSCADA database. The checks compare the imported content with the configuration that exists for the SCADAPack x70 Device Configuration item and any Analog, Digital, and/or Counter Configuration items that reference that Device Configuration item. Diagnostic messages are displayed for any incompatibilities that are detected . - If any incompatibilities are detected, address these as appropriate.
Once you have imported a manifest configuration file into ClearSCADA, you can use the SCADAPack x70 Device Configuration item's status attributes to view information about the imported manifest (see Status Attributes that are Specific to SCADAPack x70 Device Configuration Items).
If using this pick action with the Automation Interface, you need to specify the method name ImportRTZ.