SCADAPack x70

Port Function PPP/TCPIP

This port is used for TCP/IP communications. The port can be used for any enabled TCP/IP Service and DNP3. If this port Function is selected, you need to enable and Configure TCP/IP Services. This port function is only available for Serial Ports 1 and 2.


Disclaimer

ClearSCADA 2017 R3