SCADAPack x70

Specify the Point's Modbus Register Address

The Modbus tab on the Forms of SCADAPack x70 Analog, Digital, and Counter Configuration items contains a Modbus Register field.

Use the field to specify the Modbus register to which the point's values are to be mapped in the SCADAPack x70 device.

The valid Modbus register addresses are:

Value Type Address Range Description
Input values 30001-39999 Read-only input registers
Output values 40001-49999 Read/write holding registers

Disclaimer

ClearSCADA 2017 R3