SCADAPack x70

Which Driver?

ClearSCADA can communicate with SCADAPack devices using one of several drivers. The driver that you need to use depends on the type of SCADAPack device(s) with which ClearSCADA is to communicate.

If ClearSCADA is to communicate with SCADAPack x70 devices using the DNP3 protocol, your system needs to run the DNP3 driver, along with the SCADAPack x70 extension driver. Refer to the rest of this driver guide and the ClearSCADA Guide to the DNP3 Driver for information on configuring your database accordingly.

In order for ClearSCADA to communicate with other series of SCADAPack devices, your system needs to run other drivers:

Further Information

Supported Drivers and Protocols.


Disclaimer

ClearSCADA 2017 R3