Configure the Common Point Properties

Use the fields at the top of the <Point Type> tab to configure the point properties that are common to SE RPC points.

The following fields are common to SE RPC analog and digital input points. For fields that are not described here, see the relevant point configuration section within this guide.



Disclaimer

ClearSCADA 2017 R3