Real Time Clock Errors

Associated with: SE Rod Pump controllers

This status attribute indicates whether the controller’s time has drifted significantly from the system time. (The maximum allowable time difference is specified on the Outstation Form (see Specify Whether ClearSCADA Sets the Controller’s Clock).)

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R3