Configure the SQL Export Properties

Use the fields on the SQL Export tab of the SQL Export Form to configure the settings that define the data that is to be exported, along with the format and location to which that data is to be exported.


The SQL Export tab includes fields that enable you to:


Disclaimer

ClearSCADA 2017 R3