DistanceFunctions.Distance Function

The DISTANCE function calculates the distance between any two locations.

Format

DISTANCE ( <location> TO <location> )

{fn DISTANCE ( <location>, <location> )}

The result is a positive distance in meters between the two locations (the direction or order are not relevant).

Where Location can be one of the following:

 

The following is an example of the use of the Distance function in conjunction with the Location literal:

SELECT

NAME, GISLOCATION->GEOPOSITION, DISTANCE( LOCATION '51.476852,0' TO GEOPOSITION ) / 1000.0 AS "DistanceInKm"

FROM

CDBOBJECT

WHERE

GEOPOSITION IS NOT NULL

Also see:

Expressions.expr-primary-location.


Disclaimer

ClearSCADA 2017 R3