Expressions.expr-primary-odbc-datetime

A date, time or timestamp value

Format

{{ { D | T | TS } { 'Interval' | ? | ( IntervalExpr ) } }}

Remarks

Specifies a date, time or timestamp value.

The DATE, TIME, or TIMSTAMP keyword is followed by the DateTime value.

The DateTime value can be one of the following:

The resulting string is interpreted as an SQL date, time or timestamp literal. The following table describes the required format for each type:

Type Format
D YYYY-MM-DD
T HH:MM:SS[.FFFFFF]
TS YYYY-MM-DD HH:MM:SS[.FFFFFF]

For T and TS types, the fractional seconds part [.FFFFFF] is optional

Example:

{D '2007-01-31'}

{T '12:55:00.000'}

{TS '2007-01-31 12:55:00.000'}


Disclaimer

ClearSCADA 2017 R3