command-delete

Deletes row(s) from a table

Format

DELETE FROM Table [ WHERE bool-condition ]

Remarks

NOTICE

UNEXPECTED BEHAVIOR OF APPLICATION

Be aware that this command will include Group Templates if they exist in the database and are matched by the WHERE clause. Take care to exclude Group Templates when using the command to delete rows from Group Instances. Likewise, take care to exclude Group Instances when using the command to delete rows from Group Templates.
Failure to follow these instructions can result in unexpected or incomplete configuration changes.

The searched DELETE command deletes row(s) from a table. The operation is multi-row, in that zero or more rows will be deleted from a table in a single operation. The optional WHERE clause defines a condition, which identifies which rows will be deleted.

CAUTION: Omitting the WHERE clause will delete all rows from a table.

Example:

DELETE

FROM CDBPoint

WHERE FullName = 'System.Obsolete Point'


Disclaimer

ClearSCADA 2017 R3