AlarmBanner.AddMenuSeparator

The AddMenuSeparator function allows a script to add a separator line to the context sensitive menu that is available via the Alarm Banner in ViewX. The AddMenuSeparator function is only available for use in Alarm Banner scripts.

Syntax

AlarmBanner.AddMenuSeparator

Description

Adds a separator line below a menu item in the context sensitive menu that is available for alarms in the Alarm Banner. The separator line is added below the last menu item that appears before the AddMenuSeparator function in the script.

Arguments

None.

Returns

None.

Example:

In this example, the AddMenuSeparator function is used to add a separator line between the "Print Alarm Details" and "Display Alarm Form" options on the context sensitive menu for the Alarm Banner:

Function BuildAlarmMenu

AlarmBanner.AddMenuItem "Show Alarm Details","AlarmInfo"

AlarmBanner.AddMenuItem "Print Alarm Details","PrintAlarmInfo"

AlarmBanner.AddMenuSeparator

AlarmBanner.AddMenuItem "Display Alarm Report Form","DisplayAlarmForm"

End Function


Disclaimer

ClearSCADA 2017 R3