AlarmBanner.Alarms
The AlarmBanner.Alarms property represents a collection of the alarms currently in the Alarm Banner. It is only available for the Alarm Banner object and so only applies to Alarm Banner scripts.
Syntax |
AlarmBanner.Alarms |
Description |
Represents the alarms currently in the Alarm Banner in ViewX. |
Arguments |
None. |
Returns |
Alarm Collection. |
Example:
In this example, the function AllAlarms calls the PrintAlarmInfo function for the alarms in the Alarm Banner. The PrintAlarmInfo function would be defined elsewhere in the script and would define what alarm information from each alarm is printed.
Function AllAlarm
for each A in AlarmBanner.Alarms
PrintAlarmInfo A
Next
End Function
The letter A represents each alarm in the collection. A is simply a variable and you can use any letter or word to represent each alarm.