Form.AddSlider
The Form.AddSlider function allows you to add a slider control to the Form
Syntax |
Form.AddSlider(X, Y, Width, Value) |
Description |
Adds a slider control to a Form. |
Arguments |
X {integer} Represents the horizontal position of the slider on the Form—the position on the 'X-Axis'. Y {integer} Represents the vertical position of the slider on the Form—the position on the 'Y-Axis'. Width {integer} Defines the width of the slider. Value {integer} Defines the initial position of the slider when the slider is first displayed. |
Returns |
Slider Control Object Slider Control Objects have common Control Object Properties as well as their own specific properties that can be used in the script (see Slider Properties). |
Example:
Set Slider = Form.AddSlider( 1, 1, 50, 0)
This creates a slider that is positioned at 1 on the X-Axis, 1 on the Y-Axis, is 50 pixels wide and has 0 as its initial value (the slider is positioned at 0 when it is first displayed).
Further Information