Form.Clear

The Clear function removes controls and so on from a Form. In effect, the Clear function works in the same way as the Init function except that it cannot specify the title for the Form. Only the Init function can specify the title.

Syntax

Form.Clear()

Description

Removes the controls from a Form.

Arguments

None.

Returns

None.

Example:

Form.Clear

Clears a Form that has been defined earlier in the script.


Disclaimer

ClearSCADA 2017 R3