ListBox.Columns

The ListBox Control Object that is returned by the AddListBox function has a Columns property. The Columns property allows you to define the number of columns in the List Box.

Syntax

ControlObject.Columns = Columns

Where ControlObject. is the name of the variable (declared in your script) that is used to store the List Box Control Object that is returned by the AddListBox function.

Description

Sets the number of columns in the List Box.

Arguments

Columns {integer}

Defines the number of columns for the List Box.

Returns

Integer

Example:

ListBox.Columns = 2

Where:

  • ListBox is the name of the variable used to store the List Box Control Object that is returned by the AddListBox function (which would be defined earlier in the script)
  • Columns = 2 sets the List Box to have 2 columns.

Disclaimer

ClearSCADA 2017 R3