Mimic.Print

The Mimic.Print function allows the script to print the Mimic on which the script is running.

Syntax

Mimic.Print()

Description

Prints the Mimic on which the script is running.

Arguments

None

Returns

None


Disclaimer

ClearSCADA 2017 R3