Mimic Functions

The Mimic functions that you can use in your Mimic scripts allow you to utilize the print feature of Mimics as well as some navigation features, including Go Back and Go Forward.

Each Mimic function references a Mimic object. So, in your script, you need to use the following format to reference a Mimic function:

Mimic.<function name>

For more information about the Mimic functions that you can use, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3