Server.RootObject
            The RootObject property is a server property that represents the top level item in the database.
| Syntax | 
                             Server.RootObject  | 
                    
| Description | 
                             Represents the top level of the database (the Root of the database).  | 
                    
| Arguments | 
                             None.  | 
                    
| Returns | 
                             ServerObject A ServerObject is a ClearSCADA specific script object that has its own functions (see ServerObject Functions ) and properties (see ServerObject Properties) which can be manipulated.  | 
                    
Example:
The following script is used to display a message box that contains the name of the root object:
Set ServerRoot = Server.RootObject
MsgBox ServerRoot.Name
Where:
- ServerRoot is the name of the variable used to store the ServerObject that is returned by the RootObject property.
 - MsgBox ServerRoot.Name instructs the script to display a message box that contains the Name value of the ServerObject that is stored by the ServerRoot variable (this is the ServerObject that is returned by the RootObject property).