Time
The Alarm.SelectedAlarms and Alarm.Alarms properties both return an alarm collection and each alarm in the collection has a Time property. The Time property represents the time at which the alarm was raised.
Syntax |
Time |
Description |
Returns the time at which the alarm was raised. |
Arguments |
None. |
Returns |
Time {DateTime}. The time stamp for the alarm. |
Example:
In this example, Alarm.Time is used to return the time stamp of the selected alarm. The time stamp is displayed in a message box next to the text "Time", and the severity description, the alarm item’s full name, and the name of the logged on user are also shown.
Function ShowAlarmInfo( Alarm )
MsgBox "One Alarm Selected", "Severity " & Alarm.SeverityDesc & ", Time " & Alarm.Time & ", logged on user name " & Alarm.Server.Username & ", Object name " & Alarm.Object.Fullname
End Function