Web User Account

WebX does not use this account and you must log on using a valid configured user account.

The Web user account is a built-in user account. It is used whenever a user accesses ClearSCADA via a web interface such as Original WebX without logging on (see WebX Client). By default, the Web user has read-only permissions.

In some situations, the Web user may need specific permissions. For example, you may decide that web users need to be able to interact with alarms. To make this possible, you will need to configure the Web user account.

Further Information

Built-In User Accounts.

Configuring the Guest User Account.

Allocating Security Permissions.


Disclaimer

ClearSCADA 2017 R3