Communications Logging Status on Lists
            The Channels List uses color to indicate the logging status of channels. The background color of each channel's row represents the logging status—if it is white, logging is disabled for the channel; if it is dark yellow/mustard, logging is enabled for the channel.
                
            
The change of color is a visual indication of logging being enabled. This can act as a reminder that logging needs to be disabled (it should only be enabled when you need to monitor communications).
For information on accessing Lists, see see Display a List in the ClearSCADA Guide to Lists.