Delete an ODBC Table Link

If you need to remove an existing ODBC Table Link:

  1. Access the ClearSCADA Server Configuration Tool (see Accessing the ClearSCADA Server Configuration Tool)
  2. Expand the SQL Query Configuration branch.
  3. Select the Linked ODBC Tables branch to display the Linked ODBC Tables section.
  4. Right-click on the link that you want to remove, and then select Delete from the context sensitive menu.
    The Linked ODBC Table window is deleted.

As an alternative to step 4, you can select the table link that you want to remove, and then press the Delete key.


Disclaimer

ClearSCADA 2017 R3