ICMP Polls

The ICMP Polls category shows the status of ICMP 'pings' between the main and standby servers. This information is useful when investigating the connections between the ClearSCADA servers—if the ICMP ‘pings’ are unsuccessful, this would indicate that ClearSCADA could not transmit the ‘pings’, which may be due to abnormal network conditions or because the other server is not running ClearSCADA.

The ICMP Polls category provides the following information:


Disclaimer

ClearSCADA 2017 R3