Information
            The Information category provides status information about the current status of the server's hardware and software.
                
            
The Information category provides a variety of information about the server, including:
- The version of ClearSCADA that is running on the named server
 - Warnings related to database usage, see Specify the Total Lock Time per Minute Alarm
 - The current state of the server, for example, Main
 - The time that the server changed to its current state
 - The time that the server last became Main
 - The amount of available memory on the server
 - The amount of available paging file
 - The operating system that is being used
 - The server ports that are in use and the applications that are using them, for example, the WebX server
 - The number of ViewX clients and WebX clients that are connected to the server.