Log Files
            The Log Files category displays the status of the latest server log files for the database. This is useful when you need to determine whether a log file contains the latest logged data.
                
            
The status information for the log files is categorized as:
- File Base—The location of the log file.
 - Curr File—The number of the latest log file.
 - File Size—The size of the latest log file.
 - Max Size—The largest permitted size for the log file The log file cannot exceed this size; when there is more data, an additional log file will be created.
 - Pend Msg—The number of messages waiting to be flushed to disk.
 - Telnet Port—The port on which the Telnet server is running (or - if the Telnet server is not running). For more information, see Define the TCP/IP Port for Telnet Server.
 - Clients—Indicates whether any Telnet clients are connected to the Telnet server.
 - Last Message—The last message stored in the log file (the message and its time stamp).