Primary Assign

Associated with: Simatic S7 channels

The Primary Assign attribute indicates whether ClearSCADA has detected a problem with the assignment of a Simatic S7 channel to its primary serial line has failed. The line is defined on the Primary Connection tab of the Channel Form (see Configure the Connection Properties).

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R3