Secondary Assign

Associated with: Simatic S7 channels

The Secondary Assign attribute indicates whether ClearSCADA has detected a problem with the assignment of a Simatic S7 channel to its secondary serial line. The line is defined on the Secondary Connection tab of the Channel Form (see Configure the Connection Properties).

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R3