Scale Analog Values for use in ClearSCADA

Many simple drivers that support analog points also support scaling of the raw analog values into ‘engineering’ values that can be used within the ClearSCADA database. Scaling allows the raw signal values from plant to be scaled into more appropriate values for use within ClearSCADA and vice versa.

You typically configure scaling on the <Driver Type> tab of the appropriate Analog Point Form. This section explains the scaling properties that exist for analog points on many simple drivers. The driver-specific documentation mentions whether scaling is supported, or whether scaling properties differ, for the analog points on a particular driver.

Where supported by a driver, you use the fields within the Scaling section of the <Driver Type> tab to specify whether scaling of raw input values is required:


Disclaimer

ClearSCADA 2017 R3