Tabs That are Common to Many Configuration Forms

Much of the driver-specific configuration on simple drivers is undertaken using a series of configuration Forms. These Forms have a series of ‘tabs’ or ‘pages’ on which you specify different aspects of configuration.

The Forms often have a combination of these tabs, which are common to many configuration Forms:

In addition, the Forms include one or more tabs for specifying item- or driver-specific configuration. For information on configuring the properties on such tabs, see the relevant driver-specific documentation (for example, for information on the Source tab of the Modbus Source Form, see the ClearSCADA Guide to the Modbus Slave Driver).

For aspects of configuration that are common to most types of database item, see the ClearSCADA Guide to Core Configuration.


Disclaimer

ClearSCADA 2017 R3