Introduction to the Sofrel Driver

This driver is an advanced driver. It provides additional functionality to enable ClearSCADA to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring Sofrel items and features in the ClearSCADA database.

The guide also contains information for:

Document Scope

This guide explains the configuration, features and database items that are specific to ClearSCADA's Sofrel driver.

The Sofrel driver supports two Modbus transport protocols:

Sofrel outstations do not support Modbus RTU over TCP or UDP directly, so this would only be used when communicating via a 'Modbus gateway' device.

In addition the driver enables ClearSCADA to communicate with devices using two Sofrel protocols:

The driver supports the following Sofrel outstation models:

The Sofrel driver allows interoperability between RTUs (Remote Terminal Units) and ClearSCADA. A Sofrel network typically consists of a single ClearSCADA master and multiple outstations.

Most Sofrel outstations can support up to four masters, refer to the Sofrel literature for more information.

The ClearSCADA master maintains a local database that holds a copy of the data stored in each outstation.

ClearSCADA processes the data received from the outstation and:

The data sent by an outstation may be:

One of the fundamental concepts of Sofrel is that an outstation can buffer historic data. The outstation sends its buffered data to ClearSCADA when it sends a poll request to the outstation—these can be scheduled by ClearSCADA to optimize use of the communications network.

ClearSCADA supports 'report data' from the S50 range of outstations, which is a specialized form of historic data used for daily reporting.

Alternatively, the outstation can dial-in (PSTN/GSM) or make a connection (Network) to report alarms.

This guide explains how to configure Sofrel specific features and items within the ClearSCADA database.


Disclaimer

ClearSCADA 2017 R3