Source

Associated with: Many Sofrel specific database items.

The Source attribute is common to many Status displays. The attribute indicates the location at which the item resides. The information shown varies, depending on the item.

The Source attribute displays the value Undefined if the item’s configuration is incomplete, in so far as the device with which the item is associated has not yet been specified.

The Sofrel outstation Source attribute displays the configured RTU Number (and ID code if used). The RTU Number determines the Modbus address assigned to the outstation (see Configuring the Sofrel Tab)

For outstations information is displayed in this format:

RTU <RTU Number>:ID <Id1>.<Id2>

The ID code is only included if a number has been assigned in the configuration of the outstation, (see Configuring a Sofrel Outstation).

For analog input, analog output and counter point types on the Sofrel driver, information is displayed in this format:

RTU <RTU Number>:ID <Id1>.<Id2>:<Point Type> <Point Number>

For digital input and digital output points, information is displayed in this format:

RTU <RTU Number>:ID <Id1>.<Id2>:<Point Type> <Point Number> Bits <Bits>

Example:

RTU 1:AI 101

For an analog input point residing at Point Number 101 in the outstation. The outstation RTU Number is set to 1.

RTU 1:DI 1 Bits 1

For an digital input point residing at Point Number 1 in the outstation. The outstation RTU Number is set to 1.

For Report Data points (S50 Outstation only) <Point Type> shows one of the following descriptions:

The Source value displays the type of Sofrel point using these abbreviations:

Abbreviation Point Type

AI

Analog Input point

AO

Analog Output point

DI

Digital Input point

DO

Digital Output point

CI

Counter Input point


Disclaimer

ClearSCADA 2017 R3