Run the ClearSCADA Installer

To install ClearSCADA on a client or a server, you need to run the ClearSCADA installer program.

To run the ClearSCADA installer:

  1. Insert the ClearSCADA DVD. If Autorun is disabled on your PC, run the DVD manually.
  2. When the ClearSCADA screen is displayed, select the Install ClearSCADA option.

    The ClearSCADA installer runs.

  3. When you run the ClearSCADA installer, Windows may ask you if you want ClearSCADA Setup to be able to make changes to your computer. Choose Yes to allow the ClearSCADA installation to continue.

When you run the ClearSCADA installer, it checks to see if your PC has the prerequisite components installed.


Disclaimer

ClearSCADA 2017 R3