Typical Install

If you choose Typical on the Choose Setup Type ‘page’, you are presented with three options:

Server and Clients

Select this option to install the most commonly used server and client components. These include ClearSCADA server, ViewX, WebX and Data Access.

The typical Server and Clients installation contains the same components as the Full Install.

Clients

Select this option to install the ViewX Client (including the Aquis client, and the Crystal Reports component if the 32-bit Crystal Reports runtime prerequisite has been installed), WebX Client, and Data Access. These are the most commonly used client components.

Data Access

Select this option if you only want to install the WebX client and Data Access components (which allow Web, OPC, OLEDB, ODBC, and COM connections). ViewX and ClearSCADA server components are not installed when you select this option.

If you select Server and Clients, the ClearSCADA Installer displays the Custom Setup ‘page’ (see Custom Setup).

If you select Clients or Data Access, the ClearSCADA Installer displays the Ready to Install ‘page’ (see Ready to Install).

The Area of Interest Cleaner utility is installed as part of the ViewX component.


Disclaimer

ClearSCADA 2017 R3