Test Your Knowledge on Group Templates and Instances

You have created a Group Template and Group Instances and have seen how they can be used to reduce the amount of configuration work required to set up and maintain your system. But are you ready to use what you have learned? Put yourself to the test by answering these Group Template and Group Instance questions:

  1. What are the two ways you can create a new Group Template?
  2. What is the difference between a Group Template and a Group Instance?
  3. What is the difference between a Group Instance and a 'Normal' Group?
  4. What does the Property Overrides feature allow you to do?
  5. A Group Template contains a Logic program. This program is used by several Group Instances, and the Logic programs in the Group Instances are identical to the Logic program in the Group Template. An amendment needs to be made to the Logic programs. What is the quickest way to make the amendment?
  6. A point in a Group Instance needs to have its High High alarm threshold limit re-configured. The High High alarm threshold is grayed out on the point’s Form. So how do you reconfigure its High High setting?

Disclaimer

ClearSCADA 2017 R3