Introduction to the Totalflow Driver

This driver is a simple driver. It provides additional functionality to enable ClearSCADA to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is intended for engineers that are tasked with configuring ClearSCADA to communicate with supported Totalflow devices using ABB’s DB2 communications protocol.

The guide assumes an advanced level of expertise with ClearSCADA, Microsoft Windows, electronic flow measurement, and Totalflow flow computers.

Document Scope

This guide explains how to install and configure database objects on the ClearSCADA Totalflow Driver.

The guide also provides information about the example configuration that is available for importing into your database from a ClearSCADA database export (sde) file.

ClearSCADA is a flexible and extensible SCADA host platform that can be used for a multitude of purposes, including gathering data from and controlling remote devices. The ClearSCADA Totalflow Driver extends the core functionality of ClearSCADA to enable it to communicate with supported ABB Totalflow flow computers using ABB’s custom DB2 Protocol.

The ClearSCADA Totalflow driver provides a subset of the features that are available using ABB’s custom DB2 Protocol, with a bias towards gathering historical data from Totalflow flow computers.

With the ClearSCADA Totalflow Driver, you can:

ATTENTION: The level of technical information in this guide is written for users who have an advanced level of expertise with ClearSCADA, Microsoft Windows, electronic flow measurement and Totalflow flow computers.


Disclaimer

ClearSCADA 2017 R3