String Point Data Fields

In addition to the usual data fields that you would expect to find on a ClearSCADA Point object, a Totalflow String Point object also has the following data fields, which are listed in the ClearSCADA Database Schema (String Point Schema View). The name in bold at the start of each entry is also the OPC tag name.

Further Information

String Point Schema View


Disclaimer

ClearSCADA 2017 R3