Identifier Value

A TrendSpec Identifier Value is a string value that is specified without quotation marks, in the format:

<Identifier> = <Identifier value>

Example:

Format = TWENTYFOURHOUR
(for the XAXIS times to use 24-hour clock notation)

For a list of the identifier values that each optional identifier supports, see the tables in the subsections that follow; also see Supported FontStyle Identifier and Integer Values.

Identifier values are case insensitive and cannot include any character spaces.


Disclaimer

ClearSCADA 2017 R3