Min Interpolated

The Min Interpolated algorithm works in the same way as the Max Interpolated algorithm except that it calculates the lowest value in a sample rather than the highest.

For information on the Max Interpolated algorithm, see Max Interpolated.


Disclaimer

ClearSCADA 2017 R3