Min Last

The Min Last algorithm works in the same way as the Max Last algorithm except that it calculates the lowest value in a sample rather than the highest.

For information on the Max Last algorithm, see Max Last.

Related Topics Link IconFurther Information


Disclaimer

ClearSCADA 2017 R3