MinTime

The Min Time algorithm works in the same way as the Max Time algorithm except that it calculates the lowest value in a sample rather than the highest.

The results returned by the algorithm do not depend on the quality of the data. You can choose to filter the data on quality using the Qualities combo box in the Edit Source window (see Configure a Trace)

If the same minimum exists at more than one timestamp, the oldest value is used, although the quality of the data also affects which value is used.

For information on the Max Time algorithm, see MaxTime.

Related Topics Link IconFurther Information


Disclaimer

ClearSCADA 2017 R3