Trend Alarm Limits

When a point is used as the source of a Trace, it is possible to display the point’s alarm limits on the Trend. The alarm limits are useful when you want to compare the values plotted on the trace to the point’s High High, High, Low, and Low Low thresholds.

There are two types of alarm limits:

If an analog point has constant values for some of its alarm limits and uses a Time Profile for others, both types of alarm limit will be shown on Trends for the analog point.

Further Information

Hide and Show a Trace.

Hide and Show the Alarm Limits.

Time Profiles: see Configuring Time Profiles.


Disclaimer

ClearSCADA 2017 R3