SID

Many of the series of Trio radios with which ClearSCADA can communicate provide SID support.

The Stream Identifier code (also known as the Stream ID or SID code) provides the addressing mechanism for data stream routing on radio networks that use multiple message streams. The SID code identifies the message stream that is used by a particular Trio radio on such a radio network.

ClearSCADA provides these configuration properties related to SID support:

For further information on SID codes and multistream functionality, see the documentation supplied with your Trio radio equipment.


Disclaimer

ClearSCADA 2017 R3